Norgren logo

Home / Industries & Solutions / Energy / Oil & Gas / Floating Production Storage and Offloading

Floating Production Storage and Offloading

FLOATING PRODUCTION STORAGE AND OFFLOADING

FPSO

NORGREN SOLUTION

The ICO4S was originally designed specifically for the North Sea harsh environments, where it has been proven highly successful over the last 50 years.

The ICO4 has a fully stainless steel construction, high flow, low power consumption, 5 kilogram spring force and guaranteed voltage drop capability. These key features ensure the reliability of the unit in the harsh FPSO environment and durability over time as required in a limited storage vessel. The customer is typically responsible for the design, procurement and construction of many FPSOs globally.

The ICO4 has proven its reliability and resulted in specification with the customer on all the critical shutdown valves.