|
Arc Suppression
When
DC voltage is disconnected from a solenoid valve, the coil reacts
by generating its own voltage and sending a spike through
the circuit. Depending on the size of the coil and the number of
amp turns it contains, this generated voltage can be very high.
In order to suppress this spike and protect other sensitive
components in the electronic system, a diode is connected in parallel
to the coils. Once the diode is placed in the coil it will now have
a polarity. Since the diode only conducts in one direction the polarity
of the coil must be maintained so as not to burn out the diode and
eliminate the protection it is meant to provide. For ordering data
and coil availability, contact KIP.
|