Powertrain Solutions for Truck & Bus

Norgren GVT recognises the importance of complying with emissions legislation and protecting the environment without compromising performance. We are committed to pioneering solutions which will enable truck manufacturers in meet these aims - and in delivering reductions in NOx and particulate matter.

 

In fact, each one of our customized solutions is designed so that it will help you improve...

  • Engine Performance
  • Increase Turbo Efficiency
  • Increase Fuel Efficiency
  • Comply with Legislation Standards.

Powertrain Solutions...

 

ENGINE CONTROL

With petrol prices on the rise and no signs of decreasing, and the worldwide tightening of emissions regulations, it is more important than ever to have an engine which is running at its fullest potential with both high fuel efficiency and low emissions levels.

 

Norgren GVT is currently focusing on providing solutions which will help you in the following application areas:

  • Turbo Charger Motion Control
  • EGR - Motion & Fluid Control
  • Engine & Exhaust Brake Control

All of our solutions are designed to fit your needs, to achieve further systems integration and to obtain optimal control over all elements for maximum efficiency.

 

Interested in finding out more?

   

TRANSMISSION & GEARBOX CONTROL

Another important component or measure in increasing fuel efficiency as well as increasing the safety level and comfort level of the driver is the transmission system. More OEM's are looking at ways in which they can decrease the shifting forces with Manual Transmissions, and ways in which they can optimize the control of Automated Systems.

 

Norgren GVT has a number of current solutions that we have developed for our customers include XY Shift, Clutch Control and Split/Range Shift Control that help them in the above mentioned areas. We are also looking at new ways of optimizing both Manual and Automated Systems. 

 

Interested in finding out more?

 

RETARDER CONTROL

Retarders play an important role in the braking function of a vehicle, acting as both a secondary braking system and as a speed limiter, which is vital in situations such as downhill driving. Both functions are fullfilled by the Retarder which is actually a completely Wear Free system.

 

By having appropriate retarder control, you can relieve the burden which would otherwise be placed on the vehicles primary braking system. With the Retarder, no wear and tear is placed on the tires, the braking pads, the transmission or the engine. As a result, the life of the brakes, tires and related systems will be extended and overall lifetime operating costs will be reduced.

 

Norgren GVT can provide you with customized solutions for both your primary and secondary retarder that will increase the efficiency and level of control.

 

Interested in finding out more?

 

EMISSIONS CONTROL

In order to help you reduce your emissions levels, our products and solutions are in compliance with current regulations in effect around the world. Currently, we are working on the next generation of products and solutions which will be required for the next level of emission control legislation as well as what will be required beyond that.

 

Norgren GVT can design customized solutions for you, which will help in reducing emissions levels and in meeting the levels set by the legislation. The main areas in which we are working in are as follows:

  • EGR - Motion & Flow Control
  • SCR System Solutions
  • Active Filter Regeneration System Solutions
  • BioFuel System Solutions

Intersted in finding out more?

We specialize in creating Tailored Solutions for our customers. To learn more about what we can do for you, please contact us at GVT@Norgren.de or fill in our contact form.

 

<< Back to Products Home Page