This technical data will help you select the appropriate solenoid valve for your application.
The solenoid valves shown on this website are considered standard. Other types are produced for special requirements but are not listed herein. Please consult us for special requirements.
DEFINITION
The solenoid valve is a device which restricts or permits the flow of pressurised media. It converts an electrical input current into a fluid flow.
Solenoid valves are classified according to:
» Number of ways
» Type of operation
» Function
Some are specially designed to prevent the operator from coming in contact with the media. You can find them in the "dry operated valves" section.