A New Rail Dryer System and Expert Support for European train operator (1)
How manifold technology transforms modern rail engineering
Here’s a familiar problem in rail engineering: You’re designing a pneumatic control system that needs to work flawlessly for decades, handle constant vibration, and survive temperature extremes – all while fitting into a cramped space.
Don’t forget about maintenance access too, because someone’s going to need to service these components eventually.
This is where pneumatic manifolds come into their own. Instead of wrestling with dozens of separate components – each with its own mounting points, connections, and potential failure points – manifolds let you consolidate everything into one precision-engineered package.
In this article, we’ll look at how manifolds play a key role in rail system design, highlighting important manufacturing factors and sharing proven solutions already making a difference in rail operations today.
Defining pneumatic manifolds and their role in rail engineering
Pneumatic manifolds are deceptively simple devices – structured blocks or housings that route fluid flows through multiple intersecting channels. However, the engineering that goes into their design and manufacture is more precise than most would imagine.
The key process is precision cross-drilling – creating precisely positioned holes that intersect within the manifold block to form a complex network of internal pathways. These channels route fluid flows while eliminating the need for external connections.
Executing the cross-drilling process with absolute accuracy is vital. Any debris or burrs left behind during drilling could eventually damage sensitive valve mechanisms, compromising the entire system. Success in manifold manufacturing draws on deep expertise in precision machining, component integration, and rail-specific requirements – expertise that we have developed through 70+ years of fluid and motion control experience.
The role of manifolds in modern rail
From braking systems and nose cone controls to sanding mechanisms, manifolds are the glue holding together many of the pneumatic circuits responsible for a train’s safe and reliable operation. By consolidating and simplifying critical functions into a single, engineered package, manifolds deliver a host of benefits that support rail system design. These include:
Improved reliability
Rail pneumatic system failures can have serious consequences, from service disruptions to safety issues. Leaks are the primary culprit, with each individual component posing a potential failure point.
Manifolds change the equation by reducing potential leak sources. Consolidating valves, sensors, and other parts into a single integrated assembly minimizes the number of connections that could fail. When issues do arise, the systematic, modular design makes troubleshooting straightforward.
This translates to enhanced reliability across mission-critical rail systems, reducing unplanned downtime and maintenance costs. Fewer leaks, faster fixes – it's a win-win for operational efficiency and passenger safety.
Streamlined installation
Think about installing traditional rail pneumatic systems – there are numerous components, mounting points, and connections to manage. Manifolds transform this entire process, arriving as pre-engineered, plug-and-play packages that integrate seamlessly into train systems.
Cutting down the number of connections makes a dramatic difference in installation time.
There are fewer parts to handle, so technicians can work faster and make fewer mistakes.
The benefits cascade from there – simpler maintenance documentation, reduced spare parts inventory, and more streamlined operations overall. This applies to both new trains and maintenance or upgrades to those already in service, maximizing return on investment.
Compact footprints
Every cubic centimeter counts in the confined spaces of a train’s undercarriage or ceiling cavities.
Bulky individual valves, regulators, and other pneumatic components quickly consume available space.
Manifolds enable much denser component layouts by consolidating multiple functions into a single engineered assembly. Their space-saving design gives greater flexibility in positioning critical systems, opening new possibilities for optimizing overall technical architecture.
There are numerous related benefits here. For example, repositioning components for better accessibility or finding room for redundant backup systems.
Lifecycle cost savings
Manifolds create cost savings across project lifecycles, from initial procurement to ongoing maintenance.
Working with a single supplier for manifolds and pre-integrated components eliminates supply chain complexity. Combine this with faster installation, reduced labor needs, and standardized modular designs that minimize spare parts inventory – the savings quickly add up.
The financial benefits extend even further through improved reliability and space efficiency. Less maintenance downtime and more effective use of valuable undercarriage space deliver a significantly lower total cost of ownership for rail systems.
Understanding the different types of manifolds
Manifold design is far from one-size-fits-all. Different systems have different requirements, from ultimate modular flexibility to specific material properties for harsh environments.
Here are some examples of manifolds we manufacture and build:
Solid machined manifolds
Solid machined manifolds contain a network of precision-drilled channels running through a block of metal or high-performance plastic – aluminum, stainless steel, brass, or acetal.
The drilling has to be exceptionally accurate because any burrs at channel intersections could interfere with flow or damage components. We understand the importance of cross-drilling for creating clean, smooth manifold interiors that maximize flow.
You can specify different connection types in your design, from NPT to straight-thread ports.
3D printed manifolds
Using advanced 3D metal and polymer printing technology enables the creation of intricate shapes and optimized flow paths that were previously difficult or impossible to achieve. Additionally, this approach addresses challenges like obsolescence and long lead times, delivering faster and more adaptable solutions to meet evolving needs.
Custom manifolds
Custom manifolds build on solid machined or 3D printed foundations, directly integrating your valves, regulators, and other control components into the manifold block.
Real-world examples of manifolds in action
Manifold technology offers a versatile platform that can be customized to address a wide range of rail system challenges.
Whether they support mission-critical braking controls, sensitive nose cone actuation, or essential sanding mechanisms, manifolds can be engineered with the right components, materials, and configuration to deliver reliable, space-efficient solutions.
Let's look at three examples that showcase how our manifold solutions solve real engineering challenges:

Nose cone manifold
Nose cone control presents a perennial challenge – achieving absolute reliability in an incredibly tight space.
Our integrated solution combined solenoid valves, mechanical valves, and a pressure regulator in a weight-optimized package.
Importantly, we built integral manual valves to keep the nose cone working even during complete electrical failure.

Sanding system manifold
Rail safety is closely tied to traction, especially in adverse weather or on steep gradients, where sanding systems are essential.
We used manifolds to build a modular, lightweight sanding system solution that balanced performance with practicality. Every component was selected for reliable operation in harsh conditions, while the modular design kept maintenance straightforward.
The resulting system met strict rail certification standards while delivering consistent performance exactly where needed.
Unlocking the full potential of manifolds with us
Rail systems are growing more complex every year, pushing the boundaries of speed, efficiency, and performance.
Advances in rail technology bring new challenges for pneumatic systems – and this is where manifold technology truly proves its worth, bringing multiple pneumatic functions together in one elegantly engineered package.
Choosing the right manifold partner makes all the difference when it comes to designing better rail systems – improving performance, boosting reliability, and simplifying installation.
With 70+ years of precision engineering and fluid control expertise, we understand what it takes to design, manufacture, and implement these sophisticated systems in real-world conditions.
If you’re curious to learn more about how high-quality manifolds can benefit rail systems, get in touch with our team today.