What is a Motorized Valve?
What is a Motorized Valve?
Motorized valves are proportional valves that are used when the output flow needs to be precisely controlled or continuously adjusted.
What are the benefits of Motor actuated valves?
Precise control
Low power consumption
Wear resistant ceramic rotary action plates
Compact design
Suited for high temperature applications
Where are they used?
Climate control on Commercial Vehicles
Battery thermal management in Electric Vehicles
Thermal management for Fuel Cells
Coolant control in conventional powertrain vehicles
Automated production equipment
How do they work?
The valve is designed with two wear resistant ceramic discs with opposite triangular flow apertures (ball valve version also offered). Corresponding to the electric signal provided, the discs rotate over an angle of 90 ̊ opening the flow aperture. Different flow volumes can be achieved by adjusting the opening angle of the discs. The matching geometry of the pair of disks achieves a virtually linear flow characteristic.
The maintenance-free electrical servo drive consists of powerful reversible motors; with a choice between direct current (DC), synchronous and stepper motor designs to suit the type of control system available.