IECEx and Hazardous Area Zoning in Hydrogen Refuelling Stations
IECEx and Hazardous Area Zoning in Hydrogen Refuelling Stations
Explosion protection
Explosion protection is divided into two areas:
Electrical classification
Mechanical classification
Electrically actuated solenoid valves, of course belong to the electrical classification. When they are used in hydrogen service, a couple of things need to be considered. It’s up to the hydrogen station designer to define the hazardous area zoning. Three different zones are defined:
Zone 2 - hydrogen in the defined protection area is unusual, but it can happen.
Zone 1 - hydrogen needs to be considered occasionally during normal operation
Zone 0 - hydrogen is mostly present in the protection area.
For the above-mentioned zones, different protection classes are available, which makes sure there is no potential source of ignition.
The protection classes are Class ‘A’, ‘B’ and ‘C’. Protection class ‘A’ is the highest rated, followed by ‘B’ and ‘C’.
For hazardous areas in Zone 0, all components must be Class ‘A’ protection rated.
For hazardous areas in Zone 1, components must have at least, Class ‘B’ protection, but Class ‘A’ is preferable as it is higher rated.
For hazardous areas in Zone 2, all protection classes (‘A’, ‘B’ or ‘C’) can be used.
Hydrogen belongs to the fluid group “IIC”, which also includes Acetylene and carbon disulphide.
Temperature
The next criteria is the maximum permitted surface temperature. The temperature range starts at 85°C (T6 rated) up to 450°C (T1 rated). There are a couple of in-between steps, but for hydrogen the T1 class is sufficient, as hydrogen has a high ignition temperature.
Electric Rating
Overall, the minimum rating for electrified equipment for hydrogen service must include Ex IIC T6 G_.