Why Reliability Matters in Semiconductor Manufacturing and Data Centres
Behind every AI application is physical infrastructure that must perform consistently. Semiconductor facilities produce the processors on which AI depends, while data centres provide the computing capacity needed to run increasingly demanding workloads.
Although these environments serve different purposes, they share a fundamental engineering challenge: how to increase capacity while maintaining uptime, efficiency and essential services.
That challenge becomes particularly visible during maintenance. A semiconductor manufacturer, for example, may need to isolate part of a critical gas delivery system without interrupting production. A data centre operator may face a similar question when servicing cooling or utility infrastructure that supports high-density computing equipment.
These situations put reliability and maintainability at the centre of system design. The question is not simply whether an individual component will perform, but whether the wider system can remain available when equipment needs inspection, maintenance or replacement.
Why Reliability Is Becoming More Important
Growth in AI computing is increasing demand across both sides of the infrastructure chain: the manufacture of advanced semiconductors and the operation of the data centres in which they are used.
Semiconductor manufacturers are producing increasingly sophisticated devices to support AI processing, while data centres are deploying more high-performance servers to meet growing computing requirements.
Higher processing capacity brings greater demands on power, cooling, process utilities and maintenance teams. Operators must manage:
Higher power demands
Greater cooling requirements
More complex systems
More maintenance-intensive environments
Tighter uptime expectations
Reliability therefore affects more than maintenance performance. It can influence production continuity, service availability and operating cost.
Different Environments, Similar Engineering Challenges
The operational challenges facing semiconductor fabrication facilities and data centres differ, but several reliability principles apply to both.
Maintaining Continuous Operation
Many infrastructure systems cannot be easily taken offline for maintenance. In semiconductor manufacturing, interruptions to process utilities can affect production continuity and product yield. In data centres, failures within cooling, utility or supporting infrastructure can affect equipment availability and performance.
Engineers therefore need to consider how planned maintenance and equipment replacement will affect the complete system, not only the component being serviced.
Managing Risk Through Redundancy
Redundancy is one way to reduce the effect of a single point of failure. Backup components or alternative flow paths can help an essential service remain available when equipment is being maintained or replaced.
This approach can be relevant to:
Gas delivery systems
Cooling infrastructure
Utility distribution systems
Process control applications
Its value depends on how the redundant elements work within the wider system and on the operational risk they are intended to address.
Simplifying Maintenance
Reliable systems also need to be maintainable. Equipment that is difficult to inspect, isolate or service can extend maintenance activity and introduce additional operational risk.
Clear status indication, accessible isolation points and appropriate manual functionality can help maintenance teams understand system state and carry out work more efficiently.
What Reliability Looks Like in Practice
A semiconductor manufacturer needed to maintain part of a critical gas delivery system without creating unnecessary disruption to production.
To address the challenge, our engineers developed a customised valve management solution incorporating:
Redundant shut-off valves
Highly visible valve position indicators
Emergency manual valve functionality
The arrangement was designed to support maintenance activity while helping to maintain continuity of the gas supply.
The application was specific to semiconductor manufacturing, but the underlying questions are familiar across critical infrastructure: can maintenance be completed without losing an essential service, can a single failure interrupt operation, and can teams understand the status of the system clearly?

Applying the Same Principles to Data Centres
Data centres face their own reliability challenges as AI workloads and server densities place additional demands on cooling and supporting infrastructure.
Fluid control components, cooling equipment and utility systems can all influence overall availability. A failure in supporting infrastructure may affect more than the individual component involved.
Component performance therefore needs to be considered in the context of the complete cooling or utility system. System layout, isolation, monitoring and maintenance access all contribute to how readily equipment can be serviced and returned to operation.
Engineering Considerations for AI Infrastructure
The following principles can help engineering teams consider reliability across semiconductor manufacturing and data centre applications.
Design with maintenance in mind
Maintenance requirements are easier to address before equipment is installed. Engineers should consider how critical components will be inspected, isolated and replaced, and how the wider system will be affected while that work takes place.
Look beyond individual components
A reliable component cannot by itself make the complete system resilient. Identify where one failure could interrupt an essential utility and assess whether an alternative component or flow path is appropriate.
Make system status easy to understand
Clear indication and monitoring can help operating and maintenance teams identify system state and make informed decisions more quickly.
Give critical utilities appropriate priority
Gas, fluid, cooling and utility systems may sit behind the primary process, but their availability can directly affect production or computing equipment.
Designing for Continued Operation
Semiconductor facilities and data centres place different demands on their supporting infrastructure. What connects them is the need to keep essential systems available, including when maintenance is required.
Redundancy, clear status indication and accessible isolation can all contribute to that objective. Their value, however, depends on how they are applied within the wider system and the operational challenge they are intended to solve.
By considering maintenance and failure scenarios early in the design process, engineering teams can create infrastructure that is easier to operate, inspect and service throughout its working life.
Discover how our IMI engineers support reliability across semiconductor manufacturing, data centre cooling and other critical infrastructure applications.