Revolutionising Water Reclamation in Car Wash Systems
Faced with rising water and sewer costs, alongside increasing pressure to manage limited water resources efficiently, car wash operators are seeking sustainable solutions to optimise water reclamation.
With proven expertise in advanced pneumatic systems, the innovative IMI Norgren VR Valve Island was introduced, revolutionising the reclamation process by boosting reuse rates and simplifying maintenance. This blog explores how these cutting-edge solutions are shaping the future of car wash systems.
The Challenge
A leading car wash operator sought to redesign their water reclamation system to better control rising operational costs. Over the years, the cost of water and sewer services has surged, making the limited 50% efficiency of their existing reclamation system inadequate.
The goal of the redesign was ambitious: to achieve water reuse rates of 80% or higher.
However, this initiative wasn't merely driven by financial considerations. Water availability was becoming a critical issue, with many municipalities operating at full capacity. This created additional pressure on car wash operators to optimise their water usage, particularly during peak demand. The operator needed a solution that not only delivered sustainability but also reduced operating costs.
A key area of focus was improving the pneumatic control of the system’s backflushing process, which cleans the system filters at regular intervals (approximately every 20 minutes). They needed a reliable and streamlined valve solution to enable these periodic cleaning cycles smoothly.
Our Solution
Based on the operator’s long-standing confidence in IMI Norgren products, IMI was brought in to help with the redesign. Following detailed consultations, the IMI team recommended the VR series valve island as the ideal fit for the pneumatic upgrade.
The VR valve island features a compact design, which allowed the operator to centralise and organise pneumatic and electrical lines effectively. This enhanced organisation simplified installation while reducing maintenance complexity by replacing individually wired valves with a more integrated solution.
Durability was another critical advantage. The VR series valve island boasts a life expectancy of over 30 million cycles, guaranteeing dependable performance over the long term. Additionally, we supplied complementary components, including air preparation units and fittings, to further strengthen the system’s pneumatic efficiency.
Key Benefits
Our involvement played a vital role in the successful deployment of the operator’s high-performance water reclamation system. By implementing the VR series valve island, the operator unlocked several benefits that advanced their sustainability goals and operational efficiencies:
Improved Water Reuse Efficiency: Reclamation rates were significantly increased, moving beyond the industry standard of 50% and targeting 80% or higher.
Streamlined Pneumatic System: The VR valve island centralised pneumatic lines, simplifying installation and minimising maintenance requirements.
Long-Term Reliability: Designed to withstand over 30 million cycles, the VR valve island ensured consistent operation and enhanced overall system durability.
The upgraded system is now piloting advanced water reuse designs, setting a new benchmark for efficiency within the car wash industry. The VR valve island’s role in ensuring smooth operation underscores its importance in this breakthrough solution.
Advancing the Future of Car Wash Systems
IMI Norgren cutting-edge technology has helped this car wash operator redefine water reclamation standards, delivering a sustainable, high-efficiency solution. By addressing the critical challenges of cost and resource management, IMI has supported the evolution of next-generation car wash systems, paving the way for a more sustainable future in the industry.
If you’re ready to optimise your systems, contact us today to learn how our innovative solutions can help you achieve your goals.