Languages

Account

Welcome Back


My Account

View your account information including order history, saved baskets and delivery addresses.

View Account

Account

Login

Login to gain access to your account.

Forgot password?

Login

Register

Don't have an account? Register to access price and availability of your favourite Norgren products.

Register
  • Contact
  • Distributors
  • Languages
  • Login
  • 0Basket
  • Menu
  • Products
  • Industries
  • Services
  • Resources
  • About Us
  • Contact
  • Distributors
  • Login
Blog

What are the benefits of using Control Panels?

26 April 2019

Discover how control panels can help make your applications safer, neater, and more efficient.

What are the benefits of using control panels?

“Control panel” is a generic term that can be applied to a control cabinet or back-plate mounted sub-assembly delivering a bespoke pneumatic or electro-pneumatic control system solution. They are categorised alongside Manifolds and Modified Products as Custom Solutions.

Benefits of control panels

In our previous article, we looked at the differences between these options. In this article, we outline the benefits a bespoke engineered solution can bring to the client.

Benefits driven by the installation environment

Environmental factors are an important consideration in system design. For explosive environments, a suitable ATEX zone cabinet is likely to be the most efficient solution, providing secure housing for control equipment and ensuring safety within a hazardous area. Similarly, wet or dirty applications are best suited to the use of a cabinet with sufficient ingress protection levels containing all the control components.

Furthermore, by selecting appropriate materials for construction of the housing, clients can start to overcome some of their environmental challenges up front. For example, 316 Stainless steel is a popular option for the marine industry.

Benefits driven by the application

The complexity of system design can also influence choices around custom solutions. Cabinets and Back-plates provide an aesthetically pleasing and efficient way of connecting componentry whereas a manifold enables the client to fit a potentially bulky system into a drastically reduced operating envelope.   Additionally, there may be Health & Safety implications for incorrectly connected or housed system components, these can be overcome with the use of a control cabinet.

Engineering and Technical Benefits

Cabinets, panel and manifolds provide a 'one-stop-shop' custom engineered solution, as the whole package comes fully assembled, configured, tested and backed up by comprehensive documentation. The expertise and skill of a pneumatics specialist assures compatibility of all the system components and the correct integration of the solution; in other words, implementation of the current best practice. Overall, it will simplify the build and installation process, with the control system circuitry built in the workshop and not on site.

Efficiency and cost benefits

In addition to reduced commissioning times, the process simplification referred to above results in a number of benefits within the client’s own logistical process. Resources can be better utilised due to shorter engineering design and production workloads. Engineers also spend less time sourcing components, that under other circumstances may need to be purchased from multiple suppliers.

This, in turn, leads to another possible reduction in costs, through the rationalisation of the supplier base. Procurement teams can drive efficiencies by focusing more time on building closer relations with a carefully selected set of strategic suppliers. Purchasing an entire control system from one supplier can help achieve this. Finally, the multiple components of the control system and the panel can be presented as one part-number, leading to a simple one-line order.

Visit our Custom Control Solutions section to find out more.

  • You are here
Norgren Ltd, Wall Island, Birmingham Road, Lichfield, WS14 0QP, United Kingdom

We're a proud part of IMI plc

Learn more about IMI plc

Quick Links

      Help

        Legal

          Copyright © 2026 Norgren Ltd

          Norgren Ltd, Wall Island, Birmingham Road, Lichfield, WS14 0QP, United Kingdom
          • Contact
          • Register