What is a Click-on Solenoid System?
What is a Click-on® Solenoid System?
What was once actually the name of a simple yet effective fastening technology for solenoids has developed over the course of time into a complete valve range: the Click-on® dry solenoid system. A clip made from stainless steel, which is joined captively to the valve housing, holds the solenoid securely in place, irrespective to the mounting position.
A manual intervention is sufficient to fasten or replace the solenoids, with no need for tools. The Click-on® solenoid system is available for all standard voltages as well as for numerous special voltages and also with EEx or CSA approval.
When developing the Click-on® system, the valves equipped with this were also optimised further: Modern materials such as PVDF or Sandvik were used, new diaphragm and piston designs resulted, flow rates and wall thicknesses were optimised.

What are the benefits of Click-on®-solenoids?
Various solenoids, replaceable without tools
Captive retention clip made from stainless steel
Long service life
Low maintenance requirement
Simple and compact installation
Housing made from brass or stainless steel
1/4 ... 2 (ISO G/NPT) port size options


Visit our Valves section to find out more.