What is a Stroke Limiting System?

28 December 2020

This article will explain what a Stroke Limiting System is, and why it is used.

What is a Stroke Limiting System?

For the isolating valve series 845xx and 847xx is this system available as an option for adjusting the minimum and maximum flow rate.

Stroke Limiting System

Why is it used?

Stroke limiting systems are used when the valves are not to be fully closed. So they can be used very well to set a minimum flow.

It can also be retrofitted after removal of the standard position indicator.

Visit our Valves section to find out more.