What is the Pressure Equipment Directive (PED)?

20 November 2019

This article will explain what the Pressure Equipment Directive (PED) is.

What is the Pressure Equipment Directive (PED)?

The Pressure Equipment Directive (PED) is generally applicable to equipment with a working pressure greater than 0.5 bar. Valves as components of this equipment come under the scope of the directive. However, only valves above a certain nominal size are required to bear CE markings.

PED

Valves suitable for different (e.g. neutral, toxic or flammable) fluids only require CED markings above a nominal size of DN 25. Smaller valves must not bear a CE mark in accordance with the Pressure Equipment Directive. This equipment must be designed in line with standard engineering practice so that it meets the requirements of the directive. 

Almost all of the valves over DN 25 in size requiring marking should be assigned to Categories I and II. This means their design and testing is in the responsibility of the manufacturer, i.e. a company of the Norgren Group. Module H has been chosen as the related method of evaluating conformity and certified by the “nominated body” (TÜV Nord).

The products are also subject to other EU Directives such as EMC, Low Voltage, etc. The products bear a CE mark as a declaration of conformity with all of these. Where applicable (sizes > DN 25) this mark also serves as a declaration of conformity with the Pressure Equipment Directive. Category II valves are also marked with the identification number of the nominated body; CE 0045 for TÜV Nord.