What is the Protection Class (IP Protection)?

27 November 2020

This article will explain what The Protection Class (IP Protection) is, and how it works.

What is the Protection Class (IP Protection)?

The Ingress Protection (IP) code always consists of the letters IP followed by two digits. It specifies the degree of protection to DIN VDE 0470 (EN60529) provided by enclosures of electrical apparatus.

The first digit applies to protection against electric shock hazard and solid bodies, the second to protection against liquids. A letter indicating protection against access to hazardous parts may follow the last digit.

Protection Class

Which Protection Classes are available?

The individual protection codes are defined in the following table:

IP Ratings

The exact definitions from which these generalised descriptions are derived are to be found in DIN EN 60529. Special regulations have to be followed when using solenoids in hazardous areas.