Switches

Our core range of actuator position switch is the M/50 range, available as a reed switch or a solid state switch in both PNP or NPN options. These switches when fitted to a magnetic cylinder allow position sensing of the piston when fitted to the outside profile of the linear actuator.

The M/50 range come in both hard wired, in 2 5 and 10 metre lengths or a plug type – which allows easy changing of the switch. We also offer temperature resistant options as well as ATEX approved versions.