05/12/2019
What is a Compression Fitting?
This article will explain what a compression fitting is and how it works.
What is a Compression Fitting?
A compression fitting, as the name suggests, is sealed by the compression of an olive, or sleeve, against a pipe; the olive profile fits to the profile of the fitting (male to female) and completes the seal. Fittings are often nickel-plated brass or plain brass.
How do compression fittings work?
The pipe is pushed into the fitting until it bottoms against a stop. It is important to make sure that the pipe is cut square with any burrs removed and to remember to place the nut, then the olive, over the pipe before final assembly. For larger sizes of metal pipes, it is beneficial to lightly oil the pipe, olive and compression nut before tightening the joint. Ensuring the pipe remains firmly in contact with the stop, screw the nut down finger tight, then tighten a further 1 ¼ to 1 ½ full turns with a spanner, using grips to secure the fitting body. Slacken off the assembly and ensure that the groove made by the olive is even. Release the nut, then re-tighten and give an extra quarter turn.
How do I select a compression fitting?
As with all system designs, piping and fittings should be selected to allow the necessary flow without undue pressure drop; all necessary fitting shapes should be available from the range for a particular application. Other important considerations are:
working pressure – for compression fittings this is most likely limited by the pipe operating pressure
working temperature - increasing temperature will reduce the operating pressure of nylon and polyurethane tubing
working environment - both possible contaminants and ease of access for construction and maintenance
construction and maintenance - any approvals required for the application, for example, use in the Food Industry
Types of compression fitting?
Across the ranges, all standard shapes are available to complete a system design, both metric and imperial:
variety of straight adaptors
bulkhead connectors
elbow connector and adaptors
variety of tee connector/adaptors
cross connector
banjo connector
hose and tailpiece connectors/adaptors
nuts, olives and accessories
All work on the mechanical principle of connection outlined above.
Typical applications for compression fittings?
The rugged and durable nature of the fittings makes them suitable for most industrial applications.
Do I need anything else for compression fittings?
The fittings can be supplied with olive, nuts and any appropriate seals. Piping will be required for the connections to be completed. PA11 or 12 and other plasticised or unplasticised piping and other soft plastic piping. Copper annealed and half-hard; double wall brazed steel pipe. For any new system designs additional components, such as air preparation, actuators and valves will also be required.
Visit our Fittings section to find out more.