Maxseal


Maxseal

Proven in the field for over 50 years, the Maxseal brand offers extremely high quality stainless steel solenoid valves designed and manufactured with reliability and integrity in mind.


Maxseal valves perform exceptionally well in harsh environments all over the globe and are often associated with offshore oil & gas applications, but are also used onshore, particularly in coastal environments where a fully stainless steel construction is advantageous.

Maxseal products have global certifications, and due to their exceptional reliability are often found on Safety Instrumented Systems. Our products are in operation in both upstream and downstream solutions. Our latest addition to the range the ISO4-PST allows the operator to address all the requirements of partial stroke testing without compromise.

 

Something went wrong with this editor, below is the exception detail:

Value cannot be null. Parameter name: source